MLAxisReadUUnits

Pipe Network motion icon

 Function - Gets the User units per revolution value of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

UserUnitsPerRev

LREAL

 

 

Returns the Axis User Units per revolution.

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_User_Units := MLAxisReadUUnits(PipeNetwork.Axis1 )  ;