MLBlkIsReady

Pipe Network motion icon

 Function - Verifies if a Pipe Block currently has a function running.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID number of a created Pipe Block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

  • Returns FALSE if the selected Pipe Block has a function running.
  • Same return value as the .Q output of a specific function itself.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Check if the MST Pipe Block named “MASTER” has a function running 
IsReady := MLBlkIsReady( PipeNetwork.MASTER );

See Also