MLCNVConnect

 Function - Connects a converter Pipe Block to the specified axis.

  • Initializes the pipe position to the Convertor block output value.
  • Adjusts the axis Pipe Offset so that no jump in motion is generated.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Converter object.

AxisID

DINT

1 to 256

N/A

No default

ID number of an initiated Axis object.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

  • When using the Pipe Network for coordinated motion, Pipe Blocks have to be Activated, Connected, and then Powered On before move commands work.
  • The Converter block changes the incoming flow of values to continuous position output with no periodicity.
    • If a converter block is not connected to an Axis, it does not send position output values to its assigned Axis.
    • Every pipe branch must end in a converter, whether or not it is connected to a destination Axis object.

Figure 1: MLCNVConnect



  • All converters in the Pipe Network can be connected at once with the command Pipe Network(MLPN_Connect).
    This calls automatically generated code with MLCNVConnect commands for each Converter block.
    In a multi-axis program only one command can be used to connect Pipe Blocks instead of writing code for each Axis separately.


  • The converter block has the ability to control the analog output on the AKD.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Connect a converter Pipe Block named “CNV1”  to Pipe Block AXIS1
MLCNVConnect( PipeNetwork.CNV1, AXIS1 );

See Also