MLGearReadOffset

Pipe Network motion icon

 Function - Returns the Offset value of a selected Gear Block from the Pipe Network.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initialized Gear object.

Outputs

Output

Data Type

Range

Unit

Description

Offset

LREAL

 

User units

The offset value currently assigned to the selected Gear Pipe Block.

Remarks

The output of a Gear Block = Input value * Ratio + Offset.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Find the Offset value of Gear1 Pipe Block
Gear1Offset := MLGearReadOffset( PipeNetwork.GEAR1 );

See Also