MLGearWriteRatSlp
Function - Sets the Ratio Slope value of a selected Gear Pipe Block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of an initialized Gear Pipe Block. |
|
Slope |
LREAL |
No range |
1/sec |
No default |
New Ratio value to be assigned to the selected Gear Pipe Block.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
- Ratio Slope sets the limit at which step changes in ratio are implemented.
- The GEAR block output adds a position offset to the GEAR block input when using a RatioSlope.
- See RatioSlope Offset for examples.
-
-
Set the
RatioSlope < (Ratio * EtherCAT Update Rate).
The Gear block makes a jump (without a ramp) from one gear to the next when the RatioSlope is greater than the Ratio change factor multiplied by the update rate scale factor.
RatioSlope Offset
With Offset
- If MLGearWriteRatSlp is set as
MLGearWriteRatSlp (PipeNetwork.GEAR1 12, Gear1RatioSlope 500.0);to generate a ramp (instead of a step) when going from a gear ratio of 1 to 2, there is a position offset when the gear ratio settles as 2. - In this image:
- The ratio goes from 1.0 to 2.0.
- Green is PN Gear Block Output.
- Red is Gearbox Input.
|
Without Offset
If MLGearWriteRatSlp is set without a ramp, MLGearWriteRatSlp (PipeNetwork.GEAR1 12, Gear1RatioSlope 1e+301);, there is no offset.
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the Ratio Slope value of Gear1 Pipe Block to 100
MLGearWriteRatSlp(PipeNetwork.GEAR1, 100.0);
See Also