MLPmpReadLstSpd

Pipe Network motion icon

 Function - Gets the LastTravelSpeed parameter of a PMP block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of a PMP function block in the Pipe Network.

Outputs

Output

Data Type

Range

Unit

Description

LastTravelSpeed

LREAL

 

User unit/sec

Last Travel Speed of the PMP Pipe Network function block.

  • Value defined in the setup of a PMP block in a Pipe Network.
  • The value is entered in the LAST_TRAVEL_SPEED field in the Parameter tab.

Remarks

Used in the MLPmpRel function block.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

PmpLastSpeed := MLPmpReadLstSpd( PipeNetwork.PmpMaster )  ;

See Also