MLPmpWriteFstSpd
Function - Sets the FirstTravelSpeed parameter of a PMP block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID name of a PMP function block in the Pipe Network. |
|
FirstTravelSpeed |
LREAL |
> 0 (zero) |
User unit/sec |
No default |
First Travel Speed value.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
- Can be set when adding a PMP block to a Pipe Network and defining the parameters for that block.
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLPmpWriteFstSpd( PipeNetwork.PmpMaster, 300.0 ) ;
See Also