MLSyncStart

Pipe Network motion icon

 Function - Starts a synchronization of a synchronizer Pipe Block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Pipe Network Block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

Returns TRUE if the function succeeded.

Figure 1: MLSyncStart

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLSyncStart( PipeNetwork.SYN );