MLSyncStop

Pipe Network motion icon

 Function - De-synchronizes a synchronizer Pipe Block.

Inputs

Input

Data Type

Range

Unit

Default

Description

Position

LREAL

No range

User units

No default

Motion Stop Position.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

Returns TRUE if the function succeeded.

Figure 1: MLSyncStop

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLSyncStop( PipeNetwork.SYN , 120 );