MLTrigWriteDelay
Function - Sets the time the trigger block uses to compensate for the delay introduced by the sensor that captures the triggering signal.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
Identifier of the trigger block. |
|
Delay |
LREAL |
No range |
Microseconds |
No default |
Reaction time of the sensor that the trigger block has to compensate. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
- Allows the trigger block to calculate the exact moment at which a signal was triggered by the specified compensation.
- The delay compensation should include drive processing time, sensor delay, and the communication latency through the EtherCAT network.
- Electronic sensors are not able to respond immediately to a signal.
- Sensors usually require a certain amount of time to process a change of state in their input signal.
Fast Homing - Inputs
See these topics for more information:
- Example: Fast Homing with the Pipe Network Motion Engine Axis Pipe Block
- Example: Fast Homing with the PLCopen Motion Engine
- Fast Inputs with Pipe Network Motion
- Pipe Network Registration and Fast Homing
- Example: Registration Position Capture with Pipe Network Trigger Block
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also