SerializeOut
Function - Copy the value of a variable to a binary frame.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0 to 1 |
N/A |
No default |
Execute the function. |
|
Frame[ ] |
USINT |
0,+65535 |
N/A |
N/A |
|
|
Data |
ANY(*) |
No range |
N/A |
No default |
Source variable to be copied. |
|
Pos |
DINT |
0,+65535 |
N/A |
N/A |
Position in the destination buffer. |
|
BigEndian |
BOOL |
0 to 1 |
N/A |
No default |
TRUE if the frame is encoded with Big Endian format. |
(*) DATA cannot be a STRING.
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. |
|
NextPos |
DINT |
|
N/A |
|
Remarks
- Used to build a communication frame in binary format.
- This function cannot be used to serialize STRING variables.
- The FRAME input must be an array large enough to receive the data.
- If the data cannot be safely copied to the destination buffer, the function returns 0 (zero).
- The function returns the position in the destination frame after the copied data.
- The return value can be used as a position for the next serialization.
This function copies these number of bytes to the destination frame:
| Bytes | Description |
|---|---|
|
1 byte |
BOOL, BYTE, SINT, and USINT variables. |
|
2 bytes |
INT, UINT, and WORD variables. |
|
4 bytes |
DINT, DWORD, REAL, and UDINT variables. |
|
8 bytes |
LINT and LREAL variables. |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
Not available.
ST Language Example
Q := SERIALIZEOUT (FRAME, DATA, POS, BIGENDIAN);
See Also