SigPlay

PLCopen motion icon

 Function Block - Generate a signal defined in a resource.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

BOOL

 

 

 

Triggering command.

ID

DINT

 

 

 

ID of the signal resource, provided by the SigID function.

RST

BOOL

 

 

 

Reset command.

TM

TIME

 

 

 

Minimum duration between two changes of the output.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE when the signal is finished.

OUT

REAL

 

 

Generated signal.

ET

TIME

 

 

Elapsed time.

Remarks

  • The ID argument is the identifier of the signal resource.
    • Use the SigID function to get this value.
  • The IN argument is used as a Play / Pause command to play the signal.
    • The signal is not reset to the beginning when IN becomes FALSE.
    • Instead, use the RST input that resets the signal and forces the OUT output to 0 (zero).
  • The TM input specifies the minimum amount of time in between two changes of the output signal.
    • This parameter is ignored if less than the cycle scan time.
  • This function block includes its own timer.
    • Alternatively, use the SigScale function if you want to trigger the signal using a specific timer.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MySig (II, ID, RST, TM);
Q := MySig.Q;
OUT := MySig.OUT;
ET := MySig.ET;

See Also