lim_alrm

PLCopen motion icon

 Function Block - Detects high and low limits of a signal with hysteresis.

Inputs

Input

Data Type

Range

Unit

Default

Description

EPS

REAL

 

 

 

Value of the hysteresis.

H

REAL

 

 

 

Value of the high limit.

L

REAL

 

 

 

Value of the low limit.

X

REAL

 

 

 

Input signal.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE if the signal exceeds one of the limits.

Equals to QH OR QL.

QH

BOOL

 

 

TRUE if the signal exceeds the high limit.

QL

BOOL

 

 

TRUE if the signal exceeds the low limit.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) is used for enabling the block.
    • The output rung is the QH output.
    • The block is not called if EN is FALSE.

IL Language Example

Not available.

ST Language Example

(* MyAlarm is a declared instance of LIM_ALRM function block *)
MyAlarm (H, X, L, EPS);
QH := MyAlarm.QH;
Q := MyAlarm.Q;
QL := MyAlarm.QL;

See Also