rand
Function Block - Returns a pseudo-random integer value between 0 (zero) and (base - 1).
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
base |
DINT |
1 to 2147483647 |
N/A |
No default |
The number of possible outcomes. Example: When base is 5, there are 5 possible outcomes: 0,1,2,3,4. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Return Value |
DINT |
0 (zero) to (base - 1) |
N/A |
The generated pseudo-random number. |
Remarks
- rand uses a fast high-quality number generation algorithm.
- The algorithm is not cryptographically secure.
- It is sufficient where security is not a concern.
- There is no way to seed the random number generator.
- On first use, the random number generated is seeded by time.
- While unlikely, it is possible to receive the same pattern of generated numbers after the controller reboots.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
dieValue := 1 + rand(6);