min

PLCopen motion icon

 Function - Get the minimum of two integers.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1

ANY

 

 

 

First input.

IN2

ANY

 

 

 

Second input.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

IN1 if IN1 < IN2; IN2 otherwise.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The comparison is executed only if EN is TRUE.
    • ENO has the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := MIN (IN1, IN2);

See Also