QOR

PLCopen motion icon

Operator - Counts the number of TRUE inputs.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1   INn

BOOL

 

 

 

Boolean inputs.

Outputs

Output

Data Type

Range

Unit

Description

Q

DINT

 

 

Number of inputs being TRUE.

Remarks

  • The block accepts a non-fixed number of inputs.

FBD Language Example

The block can have a maximum of 16 inputs.

FFLD Language Example

The block can have a maximum of 16 inputs.

IL Language Example

Not available.

ST Language Example

Q := QOR (IN1, IN2);
Q := QOR (IN1, IN2, IN3, IN4, IN5, IN6);