r_trig

PLCopen motion icon

 Function Block - Rising pulse detection.

Inputs

Input

Data Type

Range

Unit

Default

Description

CLK

BOOL

 

 

 

Boolean signal.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE when the input changes from FALSE to TRUE.

Remarks

  • It is recommended to use declared instances of R_TRIG or F_TRIG function blocks.
    • This is to avoid contingencies during an Online Change.

Truth Table

CLK

CCLK (prev)

Q

0

0

0

0

1

0

1

0

1

1

1

0

FBD Language Example

FFLD Language Example

  • In the FFLD Language, ]P[ and ]N[ contacts can be used.
  • The input signal is the rung.
  • The rung is the output.

IL Language Example

Not available.

ST Language Example

(* MyTrigger is declared as an instance of R_TRIG function block *)
MyTrigger (CLK);
Q := MyTrigger.Q;

See Also