DTSetNTPServer
Function Block - Set the NTP server address.
This function block is specific for PCMM2G only.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, request to set the NTP server address. |
|
NTP Server |
STRING |
No range |
N/A |
No default |
The address of the NTP server used for clock synchronization. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
No range |
N/A |
Indicates the error if the Error output is set to TRUE. Error Codes
|
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// configure the NTP server address
Inst_DTSetNTPServer( bSetNTPServer, NTPServer );
if Inst_DTSetNTPServer.Done then
bSetNTPServer := false;
bError := Inst_DTSetNTPServer.Error;
ErrorID := Inst_DTSetNTPServer.ErrorID;
end_if;
See Also