bin_to_bcd

PLCopen motion icon

 Function - Converts a binary value to a Binary Coded Decimal (BCD) value.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

DINT

 

 

 

Integer value.

Outputs

Output

Data Type

Range

Unit

Description

Q

DINT

 

 

  • Converts a binary value to a Binary Coded Decimal (BCD) value.
  • Value converted to BCD or 0 (zero) if IN is less than 0 (zero).

Remarks

  • The input must be positive.

Truth Table

IN

Q

-2

0 (invalid)

0

0

10

16 (16#10)

22

34 (16#22)

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE. 
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

Not available.

ST Language Example

Q := BIN_TO_BCD (IN);

See Also

bcd_to_bin