root

PLCopen motion icon

 Function - Calculates the Nth root of the input.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL

 

 

 

Real value.

N

DINT

 

 

 

Root level.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL

 

 

Result: Nth root of IN.

Remarks

None

FBD Language

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE. 
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := ROOT (IN, N);