CycleStop
Function - Sets the application in cycle stepping mode.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
FALSE, TRUE |
|
|
Condition. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
TRUE if performed. |
Remarks
- This function turns the Virtual Machine in Cycle Stepping mode.
- Restarting normal execution is performed using the debugger.
- The VM is set in Cycle Stepping mode only if the IN argument is TRUE.
- The current program and any sub-programs called by the current program execute to the end of their cycle.
- Other programs are not executed.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also