LoadString
Function - Loads a string from the active string table.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
|
|
|
ID of the string as declared in the string table. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
Loaded string or empty string in case of error. |
Remarks
- This function loads a
string from the active string table and stores it in a STRING variable.
- The StringTable function is used for selecting the active string table.
- The ID input (the string item identifier) is an identifier declared within the string table resource.
- You don't need to define this identifier again - the system does it for you.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Q := LoadString (ID);
See Also