HToA
Function - Converts and integer to a string using hexadecimal basis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
DINT |
|
|
|
Integer value. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
String representing an integer in hexadecimal format. |
Remarks
None
Truth Table
|
IN |
Q |
|---|---|
|
0 |
'0' |
|
18 |
'12' |
|
160 |
'A0' |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
Not available.
ST Language Example
Q := HTOA (IN);
See Also