replace

PLCopen motion icon

 Function - Replace characters in a string.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

STRING

 

 

 

Character string.

STR

STRING

 

 

 

String containing the characters to be inserted in place of the NDEL removed characters.

NDEL

DINT

 

 

 

Number of characters to be deleted before insertion of STR.

POS

DINT

 

 

 

Position where characters are replaced.

Outputs

Output

Data Type

Range

Unit

Description

Q

STRING

 

 

Modified string.

Remarks

  • The first valid character position is 1.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := REPLACE (IN, STR, NDEL, POS);

See Also