StringToArray / StringToArrayU
Function - Copies the characters of a STRING to an array of SINT.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
SRC |
STRING |
|
N/A |
No default |
Source STRING. |
|
DST |
SINT |
|
N/A |
No default |
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
DINT |
|
N/A |
Number of characters copied. |
Remarks
This function:
- Copies the characters of the SRC string to the first characters of the DST array.
- Checks the maximum size destination arrays and reduces the number of copied characters if necessary.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
Not available.
ST Language Example
Q := StringToArray (SRC, DST);
See Also