TMU / TMUsec

PLCopen motion icon

 Function Block - Up-counting stop watch (seconds).

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

BOOL

FALSE, TRUE

 

 

The time counts when this input is TRUE.

RST

BOOL

FALSE, TRUE

 

 

Timer is reset to 0 (zero) when this input is TRUE.

PT

TIME

 

 

 

Programmed time. (TMU)

PTsec

UDINT

 

 

 

Programmed time. (TMUsec - seconds)

Outputs

Input

Data Type

Range

Unit

Description

Q

BOOL

FALSE, TRUE

 

Timer elapsed output signal.

ET

TIME

 

 

Elapsed time. (TMU)

ETsec

UDINT

 

 

Elapsed time. (TMU - seconds)

Remarks

TMUsec is identical to TMU except that the parameter is a number of seconds.

  • The timer counts up when the IN input is TRUE.
    • It stops when the programmed time is elapsed.
  • The timer is reset when the RST input is TRUE.
    • It is not reset when IN is false.

Time Diagram

Figure 1: Time Diagram

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* MyTimer is a declared instance of TMU function block *)
MyTimer (IN, RST, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;

See Also

TMD