TON
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
FALSE, TRUE |
|
|
Timer command. |
|
PT |
TIME |
Time Units |
|
|
Programmed time. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
Timer elapsed output signal. |
|
ET |
TIME |
Time Units |
|
Elapsed time. |
Remarks
- The timer starts on a rising pulse of IN input.
- It stops when the elapsed time is equal to the programmed time.
- A falling pulse of IN input resets the timer to 0 (zero).
- The output
signal is set to TRUE when programmed time is elapsed.
- It is reset to FALSE when the input command falls.
Time Diagram
Figure 1: Time Diagram
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung is the IN command.
- The output rung is Q the output signal.
IL Language Example
Not available.
ST Language Example
MyTimer is a declared instance of TON function block.
MyTimer (IN, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;
See Also
Function Block - On timer.