ClearCtrlErrors
Function - Clears the list of active errors and alarms on the controller.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
|
|
|
|
Enable the function. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
|
|
|
Remarks
- Only clearable errors are cleared.
- See Controller Error and Alarm Descriptions for a list of errors and alarms that may be generated.
-
-
If clearable and non-clearable errors are present and this function is called, the Output Q is turned to TRUE but the non-clearable errors remain.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Attempt to clear active controller level errors and alarms(such as E33)
IF ClearControllerErrors THEN
ClearCtrlErrors();
END_IF;