EtherNet/IP IO Scanner (Client)

The KAS Runtime includes a fully integrated EtherNet/IP client driver for exchanging CIP I/O assemblies as an EtherNet/IP scanner in your applications.

Data Exchange Configuration

A dedicated configuration tool is integrated in the KAS-IDE.

  1. Double-click the Fieldbus node in the project explorer to open it.
  2. Click the Insert Configuration icon to add the Fieldbus configuration.
    The Add Configuration dialog box opens.
  3. Select the EtherNet/IP I/O Scanner in the configuration selector. (Figure 1)
  4. Figure 1: Add Configuration dialog box

The configuration is represented as a tree:

  • EtherNet/IP I/O Scanner
    • Server (an EtherNet/IP adapter device) (*)
      • I/O Assembly (Originator to Target)
        • Exchanged Variable (*)
      • I/O Assembly (Target to Originator)
        • Exchanged Variable (*)

  • (*) The items with this mark can appear several times in the configuration.

In addition to the IO configuration, explicit messaging can be performed using these function blocks:

Server Configuration

Click the Insert Master icon to declare a server (slave adapter).

Each server is identified by its IP address and an optional Description text. (Figure 2)

Figure 2: Server dialog box


    • The Server IP address can be represented as an alias and modified externally, without using the KAS-IDE, using a custom controller configuration file.
    • See Configure Custom Project Settings.

These blocks of data are exchanged with the server for each connection:

  • Outputs (originator to target)
  • Inputs (target to originator)
  • Configuration: a static block sent to the server at connection time.

The instance number for the configuration may be specified in the properties of the server.

Edit the Configuration Data Block

While most devices do not expect any configuration it may happen that some data is required. For this, double click the server in the tree and click the Edit... button in the dialog box.

  • The configuration is entered as a list of items.
    • Use the Type button to specify the data types and number of items. (Figure 3)
  • Structured data types defined in the KAS-IDE are supported.
    • Enter values in the grid.
  • If you exchange multiple byte integers (e.g., WORD), you must specify whether the device expects little or big endian formatting.

Figure 3: Configuration data - Type dialog box

Assembly Configuration

Click the Insert Slave button () to declare a CIP I/O assembly.

Each assembly is identified by:

Identifier

Meaning

Type

Direction of the I/O assembly.

Either:

  • Originator to Target (outputs).
  • Target to Originator (inputs).

Instance

Instance of the CIP assembly.

Config.instance

The instance number of the configuration assembly.

The default value is 100.

Figure 4: Example: EtherNet/IP Scanner (client)

Size

Data size in bytes.

Connection type

Type of the CIP connection.

Can be Point To Point or MultiCast.

Priority

CIP priority:

  • Low
  • High
  • Scheduled
  • Urgent

32-bit header

Check this option if a 32-bit header is to be sent on notifications.

RPI(ms)

Minimum period for notification of changes in milliseconds.

The range is 10 - 10000 ms.

Description

Optional description text.

Configuring Variables

IEC 61131-3 variables may be mapped on the data of the assembly.

Each variable must have these specifications:

Identifier

Meaning

Symbol

The name of the IEC 61131-3 variable.

Offset

Offset in bytes in the assembly data.

Bit

Bit offset in the selected byte if format is Bit.

Format

Format of the data in the assembly

Mode

Kind of data exchanged through the variable:

  • Data Exchange: A type of input or output data in the assembly.
  • Server OK: Indicates the status of the IP connection to the server.
  • I/O connection OK: Indicates the status of the CIP I/O connection.
  • Last UCMM error: CIP code fo the last error occurred during a connection.

  • The data limit is:
    500 bytes of data maximum O(originator)->T(target) and
    500 bytes of data maximum T(target) -> O(originator).
    This is based on the EtherNet/IP specification.