Create a CAM Profile

  1. In the Project Explorer, right-click the Profiles item and click the New profile command.

    Cam - Add New Profile

  2. Figure 1: Cam - New Profile

  3. A new profile named Profile is created with default parameters.
  4. Right-click the new profile to rename it or change its properties.

    Cam - Define Profile Filename

  5. Figure 2: Cam - Define Profile Filename

  6. Click the new profile to edit it.

CAM Profile Parameters

Field

Description

Profile name

The name of the Profile which is:

  • Shown in the Project Explorer
  • Used in the Properties of the CAM Pipe Block.
  • See Use Cam Profiles for more information.

Master/Input Offset

Master/Input Scale

Slave/Output Offset

Slave/Output Scale

Offsets and scales on the X and Y axes transform the normalized profile into the output profile as shown in these images:

Cam - Normalized Profile

Figure 3: Cam - Normalized Profile

Cam - Output Profile

Figure 4: Cam - Output Profile

See Four Parameters Transforming the CAM Profile for more information.

Four Parameters Transforming the CAM Profile


  • When a CAM Profile property is changed, a dialog box indicates the progression of the operation.

See Also