Distributed Clock tab

This tab is used to change settings related to the Distributed Clock for all Kollmorgen and third-party devices (both discovered and manually added).

Figure 1: Distributed Clock tab

Element

Description

Distributed Clock Profile

Select the Distributed Clock (DC) operation mode.

These modes cannot be edited.

FreeRun, DC unused, SM-Synchronous

  • Device cyclic operation is triggered by the EtherCAT master’s SyncManager via the cyclic frame.
  • Devices are not synchronized by the reference clock.

DC-Synchron, DC for synchronization, DC-Synchronous

  • Device cyclic operation is triggered by the local distributed clock.
  • Devices are synchronized by the reference clock.

DC-Synchron (input based)

  • As DC-Synchron mode, with the cyclic start time so it coincides with other input slaves in the EtherCAT system.

Master Cycle Time

Base interval in microseconds and is used by the master.

This is changed and automatically updated by changing the Cycle Time value on the EtherCAT Master Settings tab tab.

Sync Unit 0

Cycle Time

  • Sync Unit Cycle: Unit is synchronized relative to the Master Cycle Time
  • User defined: Unit has its own interval

Shift Time

  • Unit is adjusted by the shift time

Sync Unit 1

Cycle Time

  • Sync Unit Cycle: Unit is synchronized relative to the Master Cycle Time
  • Sync 1 Cycle: Unit is synchronized relative to the First Sync Unit
  • User defined: Unit has its own interval

Shift Time

  • Unit is adjusted by the shift time

  • Some or none of the content is available in these scenarios:

    • The Sync 0 or Sync 1 parameter is not present.
    • Distributed Clock is not supported by the device.
    • The ESI file is missing.

Oversampling Devices

Some EtherCAT devices have oversampling features.

  • An oversampling device is able to record (input) or provide (output) signals at a higher rate than the EtherCAT cycle time.
  • This rate is called the oversampling factor.
  • Example: Using an oversampling factor of 10 and an EtherCAT cycle time of 1ms (1Khz), an input device can record values every 100µs (1000 divided by 10).

Oversampling devices have as many PDO objects in their cyclic frames as the oversampling factor to achieve the higher rate.

  • Each of these PDO objects corresponds to one sample.
  • Example: An output device with an oversampling factor of 4 has four PDO objects:
    • Output 1, Output 2, Output 3 and Output 4.

The oversampling factor is tied to the Distributed Clock Profile.

A warning appears next to the DC profile selection box in the Distributed Clocks tab when a device has oversampling features. (Figure 2)

Figure 2: Warning message of device with oversampling.

Changing the Distributed Clock Profile automatically changes the PDO selection.

  • All PDOs corresponding to the selected Distributed Clock Profile and its according oversampling factor are selected.
  • These maps are discarded if one or several PLC variables were mapped to a PDO that is no longer selected.