Manage a Project
- The New command in the File menu uses a wizard to help you to define the project.
- The Open... command opens a window to let you navigate your system and retrieve previous projects.
- The Save command saves your entire project.
- The Save As... command allows you to save your project with a custom name and location.
-
-
Choose a safe folder for your project.
Never select the Installation repository.
The Close command prompts you to save first if some modifications have not been saved.
-
-
When a project is already open, and you try to create or open another one, KAS-IDE shows a message asking you to save your project before it is closed.
The Print... command is used to create documentation containing editors' programs or diagrams.
See Menus and Toolbar Overview.
-
-
Use the Recent Projects command in the File menu to open the last four projects.
When editing your project, the KAS-IDE has these restrictions:
- You cannot work with several projects in parallel.
- Multiple instances of KAS-IDE can be used as a work-around.
- Modifications that impact the project structure cannot be reversed with the Undo command.
- Use the Save As command first to create a backup.
- No guarantee is provided by the KAS-IDE with respect to the project file's integrity.
- This means that, if you modify your data from outside the KAS-IDE, you can spoiled your project.
Use a Version Control System
To ensure integrity of your project files, you have to rely on tools to control versions.
Generally, such tools also have facilities for:
- Backup management.
- Multi-users or multi-site development.