PDO Restrictions and Compiler Errors
- Restrictions for AKD Devices
- Restrictions for AKD2G Devices
- Restrictions for Kollmorgen Essentials Drive Devices
- Restrictions for All Other Devices
Restrictions for AKD Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for AKD devices:
- The maximum byte count for the content of an individual PDO (both selected and unselected) is 8 bytes.
- The PDO content Size field is highlighted in red if the Editable PDO content size is greater than 8 bytes.
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 32 bytes.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) depends upon the firmware.
Firmware Version
Byte Limit
Notes
v1-17 or later
32 bytes
This is the byte limit when the EtherCAT parameter ECAT.LEGACYREV is set to 0 (zero).
v1-16 or later
20 bytes
This is the byte limit when the EtherCAT parameter ECAT.LEGACYREV is set to 1.
v1-15 or earlier
20 bytes
- The total byte count for the content of all selected Tx PDOs must be even.
- This does not apply to AKD2G devices.
- The total byte count for the content of all selected Rx PDOs must be even.
- This does not apply to AKD2G devices.
-
- The object 0x00 can be used to pad the PDO to get the total byte count to an even value.
-
- Compiler errors are generated if these restrictions are not met.
These are example compiler errors:
In AKD_1, the size of Rx PDO 0x1600 is greater than the limit: 9 > 8
In AKD_1, the total byte count for all editable Rx PDOs is greater than the limit: 39 > 32
In AKD_1, the total byte count for all editable Rx PDOs that are assigned is not even: 29
Restrictions for AKD2G Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for AKD2G devices:
- PDOs have a size constraint of 128 bytes per PDO.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- Based on the Sample Rate / Cycle Time, there is a limitation to the number of PDOobjects:
|
Sample Rate |
Cycle Time |
Max. PDOs |
|---|---|---|
|
4kHz |
250μs |
14 Rx, 14 Tx |
|
2kHz |
>500μs |
30 Rx, 30 Tx |
Restrictions for Kollmorgen Essentials Drive Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for Kollmorgen Essentials Drive devices:
- PDOs have a size constraint of 128 bytes per PDO.
- Rx PDOs
- The maximum number of Rx PDOs supported is 14.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- Tx PDOs
- The maximum number of Tx PDOs supported is 14.
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
Restrictions for All Other Devices
The KAS-IDE compiler enforces the following restriction to the editable PDOs for all devices:
- The maximum byte count for the content of an individual PDO (both selected and unselected) is 64 bytes.
Compiler errors will be generated if these restrictions are not met. Example compiler errors:
In Device_1, the size of Tx PDO 0x1A16 is greater than the limit: 66 > 64