Redundant PDO Entries
It is possible in the KAS-IDE to have the same PDO entry occur in multiple PDOs (or even in a single PDO).
- A PDO entry is uniquely defined by an Index and a Subindex.
- The name of the entry is irrelevant for identification.
In Figure 1:
- The entry defined by Index
0x6040, Subindex0, appears in the Rx PDOs0x1600and0x1604.- The entry
0x3470and subindex4appear in two different PDOs.
Redundant Rx PDO
The redundant Rx PDO would generate this compiler error:
EtherCAT: ERROR: In AKD_1, PDO object index 0x6040, subIndex 0 is redundant. It is in the following PDO(s): 0x1600, 0x1604
Attempting to export the ENI file fails with this error:
Failed to export ENI file, check the logs for more details.
Redundant Tx PDO
A redundant Tx PDO entry does not prevent a successful compilation nor generate an error when exporting the ENI file.
A redundant Tx PDO entry generates a compiler warning:
EtherCAT: Warning : In AKD_1, PDO object index 0x3470, subIndex 4 is redundant. It is in the following PDO(s): 0x1A04, 0x1B23