Safety, PDOs, and Variables
This topic is about PDOs, safety objects, and variable mapping.
- Within the PDO Selection / Mapping tab any safety-related objects are clearly identifiable by being in a yellow table. (Figure 1)
- Mapping a variable to an object is easily done by any of these methods:
- Double-click the object and select or create a variable.
- Right-click the object, select Map, and select or create a variable.
- Drag an existing variable from the Dictionary to the object.
Variables assigned to a safety object must be Read Only.
Variables that are Read/Write do not appear in dialogs and drag-and-drop does not work.
-
-
- Once a variable is assigned, there is no further validation until the project is compiled.
- That means a variable could be changed to Read/Write and still be assigned.
- When you compile the project an error is generated.
Figure 1: PDO Selection/Mapping tab with FSoE objects (in yellow).