Use the Defines List
The Defines list consists of defined constants, (an expression with a fixed value).
- Defines are:
- Both pre-defined (internal) and user-created (global and local).
- Used to determine which parts of a program's code are compiled using an
ifdefstatement.- See Conditional Compiling for more information.
- This creates more efficient code for a given machine type.
- Example: You can write a program that covers many machine types but compile for a specific machine with more efficient code.
Defined constants have these levels of scope:
|
Level |
Scope |
|---|---|
|
All the projects present on your machine. |
|
|
All the programs in your project. These are user-defined. |
|
|
Only the current program currently open. |
-
Pay special attention to the Data Types of variables used in the expression to guarantee precision when evaluating the expression. - Example: When mixing LREAL and REAL, the precision is that of REAL.
KAS-IDE