KAS Application tab
This tab is used to:
- Display general information about your project that is currently loaded on the controller.
- Start and stop the motion.
- Display the Axes run by the controller from the Axis tab tab.
- Manage log messages from the Log Configuration tab and Log Data tab tabs.
- Display User Data present on the controller from the User Data tab tab.
- Connect to a remote computer from the Shared Directory tab tab.
|
Item |
Description |
|
Version of KAS App |
This label provides information about the name and version number of the application that is in the controller.
|
|
Status of KAS App |
The state of the application, either: Started or Stopped. |
|
Start |
Default mode (warm start) where the Retain Variables are loaded at the application startup. They are Not re-initialized; whereas other variables are started with their initial values. See Retain Variables for more information. |
|
Cold Start |
Use retain variables with their default values. Such starts occurs from time to time but are few. |
|
Stop |
Stop the application. |
|
Auto-start |
Select this option to automatically start the KAS application when the controller is powered up.
|
|
Clear all errors |
Click this button to clear the error log for all axes. |