Plugging Probes, Mapping Variables
These types of variables can be mapped:
- Pipe Block variable
- IEC 61131-3 variable, which is any other variable.
- PLCopen axis values.
You can connect a probe to a variable in one of these ways:
- From the Softscope, see Map a Variable to the Oscilloscope.
- From the Dictionary, see Plug a Probe from the Dictionary.
- From the Pipe Network, see Plug a Probe from the Pipe Network.