AXIS#.BODE.PRBDEPTH

Description

AXIS#.BODE.PRBDEPTH sets the length of the PRB signal before it repeats. This applies only when AXIS#.BODE.MODE = PRB. The PRB excitation will repeat after (2^AXIS#.BODE.PRBDEPTH) / AXIS#.BODE.EXCITEGAP drive samples.

Example

Set AXIS1.BODE.PRBDEPTH to 19:

--> AXIS1.BODE.PRBDEPTH 19

Get AXIS1.BODE.PRBDEPTH (already set to 19):

--> AXIS1.BODE.PRBDEPTH 19

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

NA

Range

4 to 19

Default Value

19

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.BODE.PRBDEPTH

5001h

02h

Unsigned8

-

-

Read/Write

No