AXIS#.IL.KACCFF

Description

This value sets the gain for the acceleration feedforward (a scaled second derivative of the position command is added to the current command value) .

This parameter is valid only in the position mode (OPMODE = 2).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mARMS/(rad/s²) 

Range

0 to 10,000

Default Value

0

Data Type

Float

See Also

AXIS#.IL.FF

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.KACCFF

500ah

0dh

Signed32

-

1000:1

Read/Write

No

AXIS2.IL.KACCFF

510ah

0dh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5810

1

5810 (0x16b2)

AXIS1.IL.KACCFF

Signed32

Read/Write

Yes

71346

2

5810 (0x16b2)

AXIS2.IL.KACCFF

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.KACCFF

5810

Float

Read/Write

-