AXIS#.IL.OFFSET
Description
This value is added to the overall current loop feedforward value. A constant current command can be used to compensate for gravity.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
A |
|
Range |
|
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
AXIS#.IL.FF |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.OFFSET |
500ah |
10h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.IL.OFFSET |
510ah |
10h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5816 |
1 |
5816 (0x16b8) |
AXIS1.IL.OFFSET |
Signed32 |
Read/Write |
Yes |
|
71352 |
2 |
5816 (0x16b8) |
AXIS2.IL.OFFSET |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.OFFSET |
5816 |
Float |
Read/Write |
- |