AXIS#.MOTOR.LISAT

Description

This parameter is the quadrature axis inductance (Lqll) saturation characteristic as a function of quadrature current (Iq). It is used for q-axis current loop gain scheduling to maintain bandwidth and stability during q-axis inductance saturation.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 6.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0.2A to 2*IPEAK

Default Value

9000

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.LISAT

500bh

29h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.LISAT

510bh

29h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6231

1

6231 (0x1857)

AXIS1.MOTOR.LISAT

Unsigned32

Read Only

Yes

71767

2

6231 (0x1857)

AXIS2.MOTOR.LISAT

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.LISAT

6231

Float

Read Only

-

Related Topics

"Motor" | AXIS#.MOTOR.LQLL