AXIS#.MOTOR.NAME

Description

This parameter is the motor name.

 

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

20 chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6237

1

6237 (0x185d)

AXIS1.MOTOR.NAME

String

Read Only

No

71773

2

6237 (0x185d)

AXIS2.MOTOR.NAME

String

Read Only

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.NAME

6237

String

Read Only

-