AXIS#.MOTOR.POLES

Description

AXIS#.MOTOR.POLES sets the number of motor poles for a rotary motor. It is used for commutation control and represents the number of individual magnetic poles of the motor (not pole pairs). A motor's magnetic poles range from 0 to 510, which corresponds to 0 to 255 magnetic pole pairs. The division value of motor poles (AXIS#.MOTOR.POLES) and feedback poles (FB1.POLES) must be an integer when setting drive to enable, otherwise a fault is issued.


  • This parameter is required to be configured for all motor types.


  • For linear motors, the recommended MOTOR.POLES setting is 2.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 510

Default Value

6

Data Type

Integer

See Also

FB#.POLES

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.POLES

500bh

17h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.POLES

510bh

17h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6212

1

6212 (0x1844)

AXIS1.MOTOR.POLES

Unsigned16

Read Only

Yes

71748

2

6212 (0x1844)

AXIS2.MOTOR.POLES

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.POLES

6212

Unsigned16

Read Only

-