AXIS#.PL.KP

Description

AXIS#.PL.KP sets the proportional gain of the position regulator PID loop.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

0 to 500

Default Value

3.27

Data Type

Float

See Also

AXIS#.PL.KI

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.KP

500ch

04h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.PL.KP

510ch

04h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5908

1

5908 (0x1714)

AXIS1.PL.KP

Signed32

Read/Write

Yes

71444

2

5908 (0x1714)

AXIS2.PL.KP

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.KP

5908

Float

Read/Write

-