AXIS#.VL.FBFILTER

Description

This parameter returns the same value as AXIS#.VL.FB, filtered through a 10 Hz filter.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read Only

Units

Depends on AXIS#.UNIT.VROTARY (pg 1)

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.FBFILTER

5011h

03h

Signed32

Velocity

-

Read only

No

AXIS2.VL.FBFILTER

5111h

03h

Signed32

Velocity

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6025

1

6025 (0x1789)

AXIS1.VL.FBFILTER

Signed32

Read Only

Yes

71561

2

6025 (0x1789)

AXIS2.VL.FBFILTER

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.FBFILTER

6025

Float

Read Only

Velocity