AXIS#.IPEAK
Description
AXIS#.IPEAK returns the drive peak rated current in Arms.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Arms |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IPEAK |
5000h |
0ch |
Signed32 |
- |
1000:1 |
Read only |
No |
|
AXIS2.IPEAK |
5100h |
0ch |
Signed32 |
- |
1000:1 |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5014 |
1 |
5014 (0x1396) |
AXIS1.IPEAK |
Unsigned32 |
Read Only |
Yes |
|
70550 |
2 |
5014 (0x1396) |
AXIS2.IPEAK |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IPEAK |
5014 |
Float |
Read Only |
- |