DRV.RECPRMLIST
Description
This command returns the list of recordable parameters. You can use a recordable parameter as an input to any of the recording channels.
-
- An internal address or a registered variable can be used as input to any of the channels in addition to the list.
Examples
Code
-->DRV.RECPRMLIST AIN1.VALUE AIN2.VALUE AOUT1.VALUE AOUT1.VALUEU AOUT2.VALUE AOUT2.VALUEU AXIS1.ACTIVE ...
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-00-000 |
General Information
Variants Supported
All variants are supported.