DRV.TEMPWTHRESH

Description

This parameter returns the over temperature warning threshold of the control circuit. The value is programmed in the drive and cannot be changed.

Versions

Action Version Notes
Implemented 02-05-00-000

 

General Information

Type Read Only
Units degC
Range N/A
Default Value 85
Data Type Float

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2020

1

2020 (0x7e4)

DRV.TEMPWTHRESH

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.TEMPWTHRESH

2020

Float

Read Only

-