AXIS#.SAFE.STO.ACTIVE
Description
Indicates the Safe Torque Off (STO) state of the axis.
|
Value |
Description |
|---|---|
|
1 |
STO active (inputs +0V) |
|
0 |
STO inactive (inputs 24V) |
Context
For complete STO information refer to STO (Safe Torque Off).
For complete STO information refer to STO (Safe Torque Off).
Related safety parameters:
- AXIS#.SAFE.STO.A
- AXIS#.SAFE.STO.B
- AXIS#.SAFE.STO.REPORTFAULT
- AXIS#.SAFE.STO.RESTARTSOURCE
- AXIS#.SAFEPARAM.STO.RESTARTACKMODE
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
|
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 or 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFE.STO.ACTIVE |
5007h |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.STO.ACTIVE |
5107h |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS1.SAFE.STO.ACTIVE |
6644h |
00h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.STO.ACTIVE |
6e44h |
00h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
10002 |
1 |
10002 (0x2712) |
AXIS1.SAFE.STO.ACTIVE |
Unsigned8 |
Read Only |
Yes |
|
75538 |
2 |
10002 (0x2712) |
AXIS2.SAFE.STO.ACTIVE |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.SAFE.STO.ACTIVE |
10002 |
Unsigned8 |
Read Only |
- |